DMB Antenna

Circuit Protection of DMB Antenna



Design Notes:

Protection Application:
The communication signals carried by the antenna operate at different radio frequency, depending on the protocol – 2,600 MHz for DVB-S, 170-230/470-862 for DVB-H and DVB-T; and are less than 1.0 Vp-p in magnitude. Due to the high frequency nature of these signals, the capacitance of the suppressor must be taken into account to avoid signal attenuation. The electrical threat will be ESD.
Solution Description:
As shown at the left, a single PulseGuard suppressor is used to protect the antenna element.
Companion Solutions:
Does not apply.
Regulatory Issues:
The IEC 61000-4-2 will be the most appropriate standard that applies for this circuit. It supplies a test method for verifying that the end product is not susceptible to ESD events.
Unique Features:
Does not apply.
Application Warnings:
Does not apply.

Solutions

Solutions

  • PGB1010402

    Lead-Free 0402 Surface Mount Polymeric ESD Suppressors