Circuit Protection of Audio Lines

Circuit Protection of Audio Lines



Design Notes:

Protection Application:
For audio circuits, the signal can have a maximum value of 5.5 Vp-p, and has a maximum frequency less than 30kHz. At this frequency, the capacitance of the suppressor does not need to be taken into account. The electrical threat is ESD.
Solution Description:
SPA TVS Diode Arrays or discrete diodes can be used for layout flexibility. In the upper schematic, a two-channel array is used to minimize part count. In the lower schematic two discrete 0201 diodes are used for flexibility and the smallest size parts.
Companion Solutions:
If the customer cannot use 0201 size diodes, then the SP1003-01DTG device can be considered.
Regulatory Issues:
The IEC 61000-4-2 will be the most appropriate standard that applies for this port. It supplies a test method for verifying that the end product is not susceptible to ESD events.
Unique Features:
Application Warnings:

Solutions

Solutions

  • SP1002

    5pF, 8kV, Bidirectional TVS Array for ESD Protection

  • SP1005

    30pF 30kV Bidirectional Discrete TVS - Qualified to AEC-Q101